/******************************************************************************/
/* This file was taken from STLport <www.stlport.org> and modified by         */
/* Texas Instruments.                                                         */
/******************************************************************************/

/*
 * Copyright (c) 1999
 * Silicon Graphics Computer Systems, Inc.
 *
 * Copyright (c) 1999
 * Boris Fomitchev
 *
 * Copyright (c) 2014-2014 Texas Instruments Incorporated
 *
 * This material is provided "as is", with absolutely no warranty expressed
 * or implied. Any use is at your own risk.
 *
 * Permission to use or copy this software for any purpose is hereby granted
 * without fee, provided the above notices are retained on all copies.
 * Permission to modify the code and to distribute modified code is granted,
 * provided the above notices are retained, and a notice that the code was
 * modified is included with the above copyright notice.
 *
 */
#ifndef _STLP_LOCALE

// Basic framework: class locale and class locale::facet

#ifndef _STLP_OUTERMOST_HEADER_ID
#  define _STLP_OUTERMOST_HEADER_ID 0x1041
#  include <s__prolog.h>
#  define _STLP_LOCALE
#endif

#if (_STLP_OUTERMOST_HEADER_ID == 0x1041) && \
   !(defined (_STLP_NO_IOSTREAMS) && defined (_STLP_IMPORT_VENDOR_STD))
#  include <s__ioserr.h>

// Individual facets
#  ifndef _STLP_INTERNAL_CTYPE_H
#    include <s__ctype.h>
#  endif

#  ifndef _STLP_INTERNAL_CODECVT_H
#    include <s__codecvt.h>
#  endif

#  ifndef _STLP_INTERNAL_COLLATE_H
#    include <s__collate.h>
#  endif

#  ifndef _STLP_INTERNAL_NUM_PUT_H
#    include <s__num_put.h>
#  endif

#  ifndef _STLP_INTERNAL_NUM_GET_H
#    include <s__num_get.h>
#  endif

#if defined (__TI_COMPILER_VERSION__)
/*****************************************************************************/
/* Get definitions of LC_ALL and setlocale.                                  */
/*****************************************************************************/
#  ifndef _STLP_INTERNAL_CLOCALE
#    include <s__clocale.h>
#  endif
#endif

// those never included separately anyway
#  include <s__monetary.h>
#  include <s__time_facets.h>
#  include <s__messages_facets.h>

// some stuff for streambuf iterators ended up defined there
// Strictly speaking, _istream.h portion is only required for <iterator>, but it may break too many
// programs if we omit it
#  ifndef _STLP_ISTREAM_H
#    include <s__istream.h>
#  endif

// Convenience interfaces
#undef isspace
#undef isprint
#undef iscntrl
#undef isupper
#undef islower
#undef isalpha
#undef isdigit
#undef ispunct
#undef isxdigit
#undef isalnum
#undef isgraph
#undef toupper
#undef tolower

_STLP_BEGIN_NAMESPACE

template <class _CharT> 
inline bool isspace (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::space, c); }

template <class _CharT> 
inline bool isprint (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::print, c); }

template <class _CharT> 
inline bool iscntrl (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::cntrl, c); }

template <class _CharT> 
inline bool isupper (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::upper, c); }

template <class _CharT> 
inline bool islower (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::lower, c); }

template <class _CharT> 
inline bool isalpha (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::alpha, c); }

template <class _CharT> 
inline bool isdigit (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::digit, c); }

template <class _CharT> 
inline bool ispunct (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::punct, c); }

template <class _CharT> 
inline bool isxdigit (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::xdigit, c); }

template <class _CharT> 
inline bool isalnum (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::alnum, c); }

template <class _CharT> 
inline bool isgraph (_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).is(ctype_base::graph, c); }

template <class _CharT>
inline _CharT toupper(_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).toupper(c); }

template <class _CharT>
inline _CharT tolower(_CharT c, const locale& loc)
{ return (use_facet<ctype<_CharT> >(loc)).tolower(c); }

_STLP_END_NAMESPACE

#endif

#if (_STLP_OUTERMOST_HEADER_ID != 0x1041) || defined (_STLP_IMPORT_VENDOR_STD)
#  if defined (_STLP_HAS_INCLUDE_NEXT)
#    include_next <locale>
#  else
#    include _STLP_NATIVE_HEADER(locale)
#  endif
#endif

#if (_STLP_OUTERMOST_HEADER_ID == 0x1041)
#  include <s__epilog.h>
#  undef _STLP_OUTERMOST_HEADER_ID
#endif

#endif /* _STLP_LOCALE */


// Local Variables:
// mode:C++
// End: